990-1000008A-001

Overload Derating for UPS with IP31 Kit Installed

UPS rating

Maximum overload at 30 °C at power factor=1

Maximum overload at 35 °C at power factor=0.9

Maximum overload at 40 °C at power factor=0.9

250 kVA

210 kVA, continuous

223 kVA, continuous

210 kVA, continuous

250 kVA, for 10 minutes

265 kVA, for 10 minutes

250 kVA, for 10 minutes

300 kVA, for 1 minute

318 kVA, for 1 minute

300 kVA, for 1 minute

300 kVA

252 kVA, continuous

267 kVA, continuous

252 kVA, continuous

300 kVA, for 10 minutes

318 kVA, for 10 minutes

300 kVA, for 10 minutes

360 kVA, for 1 minute

382 kVA, for 1 minute

360 kVA, for 1 minute

400 kVA

336 kVA, continuous

357 kVA, continuous

336 kVA, continuous

400 kVA, for 10 minutes

425 kVA, for 10 minutes

400 kVA, for 10 minutes

480 kVA, for 1 minute

510 kVA, for 1 minute

480 kVA, for 1 minute

500 kVA

420 kVA, continuous

446 kVA, continuous

420 kVA, continuous

500 kVA, for 10 minutes

531 kVA, for 10 minutes

500 kVA, for 10 minutes

600 kVA, for 1 minute

637 kVA, for 1 minute

600 kVA, for 1 minute

600 kVA

504 kVA, continuous

535 kVA, continuous

504 kVA, continuous

600 kVA, for 10 minutes

637 kVA, for 10 minutes

600 kVA, for 10 minutes

720 kVA, for 1 minute

765 kVA, for 1 minute

720 kVA, for 1 minute

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.