Prepare the Backfeed Box for Cables
![]() |
---|
Hazard of electric shock, explosion, or arc flash
Do not drill or punch holes for cables or conduits with the gland plates installed,
and do not drill or punch holes in close proximity to the product.
Failure to follow these instructions will result in death or serious injury.
|
Illustrations show SP3OPT008. The procedure is the same for SP3OPT009 and SP3OPT010.
- Open the front door.
- Remove the screws and the front plate.
- Remove the gland plate.
- Drill or punch holes for cables or grommets/conduits (not provided) in the gland plate.
- Install grommets/conduits (if applicable) and refit the gland plate.
DANGER
hazard of electric shock, explosion, or arc flashEnsure that there are no sharp edges that can damage the cables.Failure to follow these instructions will result in death or serious injury.