990-92223A-001

Connect the Bypass Power Cables to the Bypass Backfeed Box for 3:3 System (Dual Mains System Only)

NOTE: Follow the UPS installation manual to remove the single mains busbars in the UPS.
  1. Connect the PE cables.
  2. Connect the UPS bypass cables (L1, L2, L3, N).
  3. Connect the bypass cables (L1, L2, L3, N).
  4. Reinstall the front plate with the screws.
  5. Close and lock the front door.

    SP3OPT008 for 3:3 System (Bypass Only)

    SP3OPT009 for 3:3 System (Bypass Only)

    SP3OPT010 for 3:3 System (Bypass Only)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?