990-91604B-001

TN-S System Single Source and Dual Mains

TN-S Single Source and Dual Mains with 3-Pole Circuit Breakers

NOTE: Refer to IEC 60364 series for general requirements and refer to local codes for specific local requirements.

TN-S Single Source and Dual Mains with 4-Pole Circuit Breakers

NOTE: Refer to IEC 60364 series for general requirements and refer to local codes for specific local requirements.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?