990-91604B-001

IT System Dual Source and Dual Mains

IT System Dual Source and Dual Mains with 3-Pole Circuit Breakers

NOTE: Refer to IEC 60364 series for general requirements and refer to local codes for specific local requirements.
NOTE:
  1. When an IT system is used for continuity of supply, an insulation monitoring device must be provided according to IEC 60364-4-41.

  2. Impedance (Z) has to be sufficiently high or be an open circuit in order to achieve low fault current.

IT System Dual Source and Dual Mains with 4-Pole Circuit Breakers

NOTE: Refer to IEC 60364 series for general requirements and refer to local codes for specific local requirements.
NOTE:
  1. When an IT system is used for continuity of supply, an insulation monitoring device must be provided according to IEC 60364-4-41.

  2. Impedance (Z) has to be sufficiently high or be an open circuit in order to achieve low fault current.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?