990-91191F-001

Connect the Power Cables in the 10-15 kVA UPS

  1. Ensure that all breakers are in the OFF (open) position.
  2. Remove the conduit box cover.

    Rear View

  3. In dual mains systems, remove the single mains cable.
  4. Route the power cables through the bottom of the conduit box.
  5. Connect the PE cable to the PE terminal.
  6. Connect the input, output, and bypass (if applicable) cables.
  7. Connect the battery cables.
  8. Reinstall the conduit box cover.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.