990-66227-001

Install E3SOPT013 on Easy UPS 3S E3SUPS20K31, E3SUPS30K31

  1. Remove the existing conduit box from the UPS.
  2. Remove the front gland plate from the glanding box E3SOPT013.

    Front View of Glanding Box E3SOPT013

  3. Drill/punch holes for power cables/conduits in the front gland plate. Install conduits (not provided), if applicable.
    DANGER
    HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Do not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the UPS.
    Failure to follow these instructions will result in death or serious injury.
  4. Connect the power cables:
    1. Route the power cables through the front gland plate.
    2. Route the power cables through the glanding box.
    3. Connect the power cables to the power terminals on the UPS according to the UPS installation manual.
  5. Install the glanding box on the UPS. Torque to 1.2 Nm.
  6. Reinstall the front gland plate on the glanding box.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?