990-66227-001

Install E3SOPT019 on Easy UPS 3S E3SUPS30K31B, E3SUPS40KHB, E3SUPS30KHB

  1. Remove the existing lower plate from the UPS.
  2. Drill/punch holes for power cables/conduits in the lower part of the gland plate E3SOPT019. Install conduits (not provided), if applicable.
    DANGER
    HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Do not drill or punch holes with the gland plate installed and do not drill or punch holes in close proximity to the UPS.
    Failure to follow these instructions will result in death or serious injury.

    Front View of Glanding Box E3SOPT019

  3. Connect the power cables:
    1. Route the power cables through the gland plate.
    2. Connect the power cables to the power terminals on the UPS according to the UPS installation manual.
  4. Install the gland plate on the UPS. Torque to 1.2 Nm.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?