990-5912E-001

Installation Procedure for Galaxy VS UPS

Single System – Single Mains

Simplified 1+1 Parallel System – Single Mains

Single System – Dual Mains

Simplified 1+1 Parallel System – Dual Mains

  1. Mount the Maintenance Bypass Panel to the Wall.
  2. Prepare the Maintenance Bypass Panel for Cables.
  3. Only in countries where required: Remove the Neutral Jumpers.
  4. Connect the Power Cables for a 3:3 UPS System.
  5. Do one of the following:
  6. Add Translated Safety Labels to Your Product.
  7. Final Installation.
For moving or decommissioning the maintenance bypass panel after installation has been completed, see Decommission or Move the Maintenance Bypass Panel to a New Location.