990-5912E-001

Connect the Signal Cables for Easy UPS 3S, Easy UPS 3S Pro, and Easy UPS 3M – Single System

  1. Remove the three disconnect device indicator lights and the disconnect device indicator light labels from the maintenance bypass panel. The disconnect device indicator lights are not supported with the Easy UPS 3S, Easy UPS 3S Pro, and the Easy UPS 3M.

    GVSBPSU20K60H and GVSBPSU80K120H

  2. Install three round blanking plugs (not provided) in the holes in the inner door.
  3. On the control terminal block, remove the internal connections for the disconnect device indicator lights (pin 1-4).
  4. On the control terminal block, modify the internal connection for the MBB AUX switch (pin 7-8) from Normally Closed (NC) to Normally Open (NO).
  5. Connect the Class 2/SELV signal cables from the control terminal block in the maintenance bypass panel to the UPS as per your configuration.
    NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables separately from the non-Class 2/non-SELV cables.

    GVSBPSU20K60H and GVSBPSU80K120H

    NOTE: There is no dedicated input contact for MBB on Easy UPS 3S. By default, use J5 configurable input contact and configure the input contact as Main CB NO.

    Easy UPS 3S

    Easy UPS 3S Pro

    NOTE: There is no dedicated input contact for MBB on Easy UPS 3S Pro. By default, use J2 configurable input contact and configure the input contact as Main CB NO.

    Easy UPS 3M

  6. Pull up the slack in the signal cables and fasten the signal cables to the cable reliefs.