990-5938B-001

Battery Circuit Breaker Box Specifications

DANGER
hazard of electric shock, explosion or arc flash
The battery circuit breaker box must only be used with the Easy UPS 3S or Easy UPS 3S Pro.
Failure to follow these instructions will result in death or serious injury.
  E3SOPT007
Battery circuit breaker LV438118+LV438135 or
LV438880
Maximum configuration 4 hour runtime
Battery type Lead-acid
Maximum battery short-circuit level (kA) 10
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?