990-5938B-001

Connect the Signal Cables for Easy UPS 3S

  1. Loosen the screws of the inner covers and lift the inner covers up and out of the battery circuit breaker box.

    Front View of the Battery Circuit Breaker Box

  2. Route the signal cables through the top or bottom of the battery circuit breaker box.
  3. Remove the cover on the battery circuit breaker.

    Front View of the Battery Circuit Breaker Box

  4. Connect the signal cables:

    Front View of the Battery Circuit Breaker Box

    1. Connect the aux switch signal cables from the empty classic battery cabinet to J6–2 and J7–1 in the UPS.
    2. Connect the shunt trip coil signal cables from the empty classic battery cabinet to J5–3 and J6–1 in the UPS.
    3. Fasten the signal cables with cable ties (provided) to the cable relief.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?