990-91190B-001

Connect the Signal Cables for Easy UPS 3S

NOTE: Route the signal cables separately from the power cables.
  1. Remove the plastic cover of the maintenance bypass switch MBB to get access to the auxiliary switches.
  2. Connect signal cables 18 AWG (not supplied) between the maintenance bypass switch MBB and UPS 1 and UPS 2. Use one of the two methods shown below.
  3. Fasten the signal cables to the cable reliefs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?