990-91190B-001

Overview of UPS System with Parallel Maintenance Bypass Panel

UIB Unit input disconnect device
SSIB Static switch input disconnect device
UOB Unit output disconnect device
MBB Maintenance bypass disconnect device
BB Battery disconnect device

Single Mains System

Dual Mains System

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?