DOCA0396EN-00

Device Characteristics

Overview

The EcoStruxure Flex-Server has security-enabling features. These features come in a preset state, and you can modify them to meet your installation needs. Qualified personnel must configure and set the EcoStruxure Flex-Server because disabling or changing settings affects the overall security robustness of the EcoStruxure Flex-Server and your network security.

To set up the EcoStruxure Flex-Server features and settings, use this guide along with the EcoStruxure Building Activate - User Guide.

EcoStruxure Flex-Server Interfaces

The EcoStruxure Flex-Server communicates through the following interface types:

  • Wired communication through:

    • One Ethernet port

    • One RS-485 port

    • Two USB Ports

  • Radio communication through:

    • Wi-Fi infrastructure

    • LoRaWAN Modem

    • Cellular/LTE Modem

Supported Protocols

The EcoStruxure Flex-Server supports the following protocols:

  • HTTPS and MQTTS (TLS v1.2)

  • CoAP over DTLS

  • BACnet MSTP and BACnet IP for communications with other Operational Technology (OT) devices

  • SNMP for communications with other Operational Technology (OT) devices

  • Modbus TCP and Modbus-RTU for communications with other Operational Technology (OT) devices

  • LoRaWAN for wireless communications with IoT devices

  • OpenVPN client for remote access (open to Schneider Electric)

  • DHCP for network IP addressing

  • DNS for network name resolution

  • NTP for time synchronization

  • WPA2 and WPA for Wi-Fi communication

Security Features

EcoStruxure Flex-Server supports the following security features:

  • Schneider Electric digitally signs the only firmware that can be installed on the EcoStruxure Flex-Server.

  • At each boot, the system validates the firmware digital signature before execution, to help ensure that it has not been tampered.

  • User passwords are stored as salted and hashed (SHA256) passwords.

  • The device has an internal clock and maintains its date and time for a few months without power.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?