Hardware Description

Panel Server Entry

Front face

Bottom

Top

       
   
  1. Panel Server status LED

  2. Multifunction button

  3. QR code to product information (including device code, credentials for use in secure claiming of Panel Server from Cloud applications)

  4. Ethernet LED 1: Speed

  5. Ethernet LED 2: Activity

  6. Ethernet communication port

  7. Power supply terminal block

  8. MAC address and serial number

For information about installation of Panel Server Entry, consult the instruction sheet available on the Schneider Electric website: NNZ76760.

Panel Server Universal

Front face

Bottom

Rear

       

Top

 
  1. Power supply terminal block

  2. Digital input terminal block (PAS600L)

  3. Panel Server status LED

  4. Multifunction button

  5. QR code to product information (including device code, credentials for use in secure claiming of Panel Server from Cloud applications)

  6. RS485 Modbus communication port

  7. Ethernet LED 1: Speed

  8. Ethernet LED 2: Activity

  9. External Wi-Fi antenna port

  10. Ethernet 1 communication port

  11. Ethernet 2 communication port

  12. Grounding connection

  13. MAC address and serial number and hardware version HW: V2.0 (for hardware version 002.000.000 only)

  14. External IEEE 802.15.4 antenna port (for HW: V2.0 PAS600, PAS600L, PAS600P only)

For information about installation of Panel Server Universal, consult the instruction sheet available on the Schneider Electric website: GEX84977

Panel Server Universal Wired by Design

Front face

Bottom

Rear

       

Top

 
  1. Power supply terminal block

  2. Digital input terminal block (PAS600LWD)

  3. Panel Server status LED

  4. Multifunction button

  5. QR code to product information (including device code, credentials for use in secure claiming of Panel Server from Cloud applications)

  6. RS485 Modbus communication port

  7. Ethernet LED 1: Speed

  8. Ethernet LED 2: Activity

  9. Ethernet 1 communication port

  10. Ethernet 2 communication port

  11. Grounding connection

  12. MAC address, serial number, and hardware version HW: V2.0

For information about installation of Panel Server Universal Wired by Design, consult the instruction sheet available on the Schneider Electric website: PKR28607.

Panel Server Advanced

Front face

Bottom

Rear

       

Top

 
  1. Power supply terminal block (PAS800, PAS800L)

  2. Digital input terminal block (PAS800L)

  3. Panel Server status LED

  4. Multifunction button

  5. QR code to product information (including device code, credentials for use in secure claiming of Panel Server from Cloud applications)

  6. RS485 Modbus communication port

  7. Ethernet LED 1: Speed

  8. Ethernet LED 2: Activity

  9. External Wi-Fi antenna port

  10. Ethernet 1 communication port

  11. Ethernet 2 communication port

  12. Grounding connection

  13. MAC address and serial number and hardware version HW: V2.0 (for hardware version 002.000.000 only)

  14. External IEEE 802.15.4 antenna port (PAS800, PAS800L)

For information about installation of Panel Server Advanced, consult the instruction sheet available on the Schneider Electric website: BQT54848

Hardware Version

The Panel Server exists in two hardware versions, depending on the model and the date of manufacture, hardware version 001.000.000 and hardware version 002.000.000.

The following models of EcoStruxure Panel Server are released with hardware version 002.000.000 (HW: V02):

  • PAS600P

  • PAS600PWD Wired by Design model without wireless communication capability

  • PAS600LWD Wired by Design model without wireless communication capability

Certain models of Universal and Advanced EcoStruxure Panel Server exist in two hardware versions: 001.000.000 and 002.000.000 (HW: V02). Both versions offer the same capabilities and functionality. For PAS600 and PAS600L, hardware version 002.000.000 allows you to add an external IEEE 802.15.4 antenna, not available for hardware version 001.000.000.

To identify the hardware version of your Panel Server, check in one of the following ways:

  • The information printed on the top of the Panel Server:

    • Hardware version 001.000.000: MAC address and serial number

    • Hardware version 002.000.000: MAC address, serial number, and HW: V2.0

  • In the Panel Server webpages at either of the following paths:

    • Settings > General > Identification > Hardware revision

    • Maintenance > Firmware update > Hardware revision

Panel Server Status LED

The LED indicates the operation mode of the Panel Server.
LED indication Description
Panel Server switched off.

Panel Server is powering on. System boots within 2 minutes.

Panel Server in normal operation.

Minor malfunction detected. Connect to Panel Server software to diagnose.

Major malfunction detected. Panel Server must be replaced.

Wi-Fi access point is available for connection.

Wi-Fi access point connection is established.

Ethernet Status LEDs

The combination of the two LEDs of one RJ45 port indicates the Ethernet communication status of the Panel Server.

Ethernet LEDs

Description

LED 1: Speed

LED 2: Activity

No Ethernet communication

10 Mb Ethernet communication active

100 Mb Ethernet communication active

Multifunction Button

Use the multifunction button to perform the following functions:

  • Initiate connection using the Wi-Fi access point (except Wired by Design models)

  • Restart the Panel Server

  • Reset the Panel Server to factory settings

Function Action LED status Indicates

Activate Wi-Fi access point

Press the multifunction button for less than 5 s

Blinking blue

The Panel Server Wi-Fi access point is available for connection.

Steady blue

The Wi-Fi access point connection is established.

Blinking fast orange

The Wi-Fi access point connection is not authorized.

Restart Panel Server

Press the multifunction button for 5 s to 10 s

Steady orange

The Panel Server is restarting.

Steady green

The Panel Server is in normal operation after restart.

Reset Panel Server to factory settings

Press the multifunction button for more than 10 s until the steady orange LED starts blinking fast.

Blinking fast orange

Reset to factory settings is initiated.

Confirm reset to factory settings by pressing the multifunction button again within 5 seconds.

Blinking fast green

Reset to factory settings is confirmed.

To cancel reset to factory settings, wait for the LED to change color.

Blinking fast red

Reset to factory settings is cancelled.

Wait for the Panel Server to restart completely.

Steady orange

The Panel Server is booting

Steady green

The Panel Server is in normal operation after reset.

QR Code

When the QR code on the front face of a Panel Server is scanned with a smartphone connected to the Internet, the Go2SE landing page is displayed.

The landing page displays:

  • Information about the Panel Server

  • A list of menus

Tamper Detection

A tamper-indicating label helps detect unauthorized physical access into the Panel Server. This label is light grey with Schneider Electric written in black.

The following figure illustrates the position of the tamper-indicating label (A) affixed on the right-hand side of the Panel Server:

Before installing, operating, servicing, or maintaining the EcoStruxure Panel Server, check the tamper-indicating label integrity.

External Wi-Fi Antenna (Optional)

The external Wi-Fi antenna is an option for:

  • Panel Server Universal (except Wired by Design models)

  • Panel Server Advanced

Use the external Wi-Fi antenna in specific use cases such as when the Panel Server is installed in a switchboard with metallic partitions and door. The antenna improves the quality of radio frequency signal.

Connect the Wi-Fi antenna (reference PASA-ANT1) at the bottom of the Panel Server and install the antenna on the roof of the switchboard.

For information about installation of the external antenna, consult the instruction sheet available on the Schneider Electric website: NNZ58425.

For information about configuring the Panel Server after installing the external antenna, refer to Wi-Fi Infrastructure.

For information about Wi-Fi communication in the Panel Server system, consult DOCA0289•• Wireless Communication Architectures With EcoStruxure Panel Server - Design Guide.

External IEEE 802.15.4 Antenna (Optional)

The external IEEE 802.15.4 antenna is an option for:

  • Panel Server Universal hardware version 002.000.000 (except Wired by Design models)

  • Panel Server Advanced

Use the external IEEE 802.15.4 antenna in specific use cases such as when the Panel Server Advanced is installed in a switchboard with metallic partitions and door and some wireless devices are located in a different place. The antenna extends the wireless network outside the switchboard.

Connect the IEEE 802.15.4 antenna (reference PASA-ANT1) at the top of the Panel Server Advanced and install the antenna on the roof of the switchboard.

For information about installation of the external antenna, consult the instruction sheet available on the Schneider Electric website: NNZ58425.

For information about configuring the Panel Server after installing the external antenna, refer to Wi-Fi Infrastructure.

For information about wireless communication in the Panel Server system, consult DOCA0289•• Wireless Communication Architectures With EcoStruxure Panel Server - Design Guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?