DUG_ELKO - SmartSocket Double 16 A_WH-00

Resetting the device

You can reset the Socket outlet to the factory default manually.

Short-press the push button 3 times (<0.5 s) and then long-press the push button once (>10 s). The LED blinks red after 10 s, and then release the push button.

Upon successful reset, the LED stops blinking. Then, the device restarts and blinks green for a few seconds.

NOTE:
  • All configuration data, user data and network data are deleted.

  • After reset, the LED turns amber, indicating that the socket is ready for pairing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.