DUG_Smart Smoke Alarm 230 V_WH-00

Interconnecting devices without Wiser Hub

The smoke alarms can be connected directly to each other via RF connections even without a Wiser Hub network.

IMPORTANT: Turn the power switch to ON position on all the devices.
  1. Identify a smoke alarm and mark it as Primary with a label supplied. Other smoke alarms are considered as Secondary.

  2. Short press the Test/Hush button 3 times within 2 s on the primary smoke alarm.


    The Standby LED turns on for 30 s once it is in pairing mode.

  3. Identify a Secondary smoke alarm and short press the Test/Hush button 3 times within 2 s.


    The Standby LED blinks 3 times on both Primary and Secondary smoke alarms indicating a successful RF connection. Then on the Primary smoke alarm, the Standby LED again turns on for 30 s.

Repeat the step 3 on all Secondary smoke alarms.

NOTE: To exit from pairing mode, short press (< 0,5 s) the Test/Hush button 3 times on the Primary smoke alarm. The Standby LED turns off indicating that the Primary smoke alarm is not in pairing mode.

IMPORTANT: To make sure you have correct interconnection, perform an interconnection test on all smoke alarms before and after installation. Refer testing the interconnected device(s).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.