DUG_SmartSensor Climate Wireless_WH-00

Checking the device history

Using the Wiser Home app, you can view the sensor history which displays room temperature and humidity values recorded as an event. The sensor records each event and stores it in the cloud.
NOTE: If the cloud connection is lost, the temperature and humidity values will not appear in the history.
  1. On the Control tab, tap All devices or a room tab where the sensor is located.
  2. On the device control panel page, tap History.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?