Pairing the device with the Wiser Hub
- On the Home screen, tap
.
- Tap >Climate > Temperature/Humidity Sensor.
- Tap Scan QR code and allow the Wiser
Home app to access your camera. Then, scan the QR code located on
the device.NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.
If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:
-
(A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid.
-
(B): Tap this option if you are unable to find the Mac Address/EUI–64 and Install code.
-
- Tap Next, short press the function key 3 times and make sure that the LED blinks amber.
- Ensure that the first battery cover is securely fastened, then install the sensor on the base plate. For more information, refer to the installation instruction.
- Tap ,
to enter the name of the sensor.
NOTE: If you are already using any of the following Wiser Heating devices, then proceed to Step 8. If you wish to use the Temperature/Humidity Sensor for temperature control in conjunction with a heating device, then proceed to Step 7.-
Wiser 16 A Relay for Temperature Control
-
ELKO - Smart Radiator Thermostat
-
Wiser Underfloor Heating Connection Strip
-
- Turn on the toggle to allow the Temperature/Humidity Sensor to measure room temperature in conjunction with your thermostat.
- Tap Next and assign the sensor to
a new room or an existing room and tap Submit.IMPORTANT: The next screen shows the Device Settings page, where you have the option to configure the settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit. For more information on device settings, refer to Configuring the device section.
After you pair the device, a success screen appears with the following options:
-
+ Add New Device: Tap to continue pairing more devices.
-
Start Using Your Device: Tap to start using the paired device.
NOTE: The success screen appears only if you are logged in as a Home Owner.Now, you can see the newly added sensor on the Control tab under the All and Room tabs.
-