DUG_SmartMove Dimmer Push_WH-01

Defining Lux settings

You can define the threshold value for Lux ranges (such as very dark, dark, bright, and very bright) of the environment. This will prevent the false detection caused by changes in the light intensity.
  1. On the Home screen, tap .
  2. Tap Devices > Lights > Motion Dimmer > Lux Level Threshold.
  3. Drag the slider bar to set the Lux threshold value.
    TIP:
    • You can also select Use the current lux value to set the current Lux level as the threshold level. If the current lux value exceeds 1023, this option is disabled.

    • To set your motion sensor dimmer to detect motion without turning on the lights, drag the slider bar to set the threshold to 0. The motion detection will still work for all purposes, but the lights will not turn on.

    The Lux level ranges are as follows:

    • Very Dark: <6 Lux

    • Dark: 6-100 Lux

    • Bright: 101-300 Lux

    • Very Bright: >300 Lux

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?