DUG_SmartMove Dimmer Push_WH-01

Google Home

You can use Google Assistant to request information or perform an action using a variety of commands.

Common Wiser commands for Google Home:

  • Inquiry: “OK, Google, is the Motion Sensor Dimmer On?”

  • Motion detection: “OK, Google, is the sensor detecting movements?”

  • Turn on/off the device: “OK, Google, turn on/off the Motion Sensor Dimmer.

  • Brightness level %: “OK, Google, increase or decrease the brightness by XX percentage”.

  • Minimum brightness: “OK, Google, set the Motion Sensor Dimmer to minimum brightness”.

  • Maximum brightness: “OK, Google, set the Motion Sensor Dimmer to maximum brightness”.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.