Configuring the device
|
A |
Device Name: Tap to change the name of the device. |
|
B |
Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. |
|
C |
RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle switch to enable the RL-LED Mode. TIP: For more information, refer
toTechnical Data.
|
|
D |
Power On Behaviour: Tap to set the default brightness level of the dimmer when it is turned on. For more information, refer to Setting up the Power On Behaviour for detailed information on each options. |
|
E |
Minimum Brightness and Maximum Brightness: This setting allows
you to set limits on the maximum and minimum brightness of the Motion
Sensor Dimmer. This is done to avoid flickering and switching off
the LED. IMPORTANT: If the light does
not begin to brighten up from 0%, adjust the minimum level setpoint
to the point where the light actually starts to brighten. Similarly,
for maximum brightness, set the maximum level based on the behaviour
of the connected light. For example, if brightness does not increase
between 80% and 100%, then set the maximum level to 80%.
NOTE: The minimum brightness must be lower than the maximum brightness.
|
|
F |
Motion Detection Sensitivity: Tap to set the sensitivity level of the sensor as per your preference. For more information, refer to Setting the detection sensitivity for detailed information on each option. |
|
G |
Motion Detection Timer: Tap to set the time for how long the light should remain On after motion is detected. For more information, refer to Setting the motion detection timer. |
|
H |
Current Lux: Displays the current Lux value of the light present in the environment measured by the sensor. Lux is a unit of illuminance that measures the amount of visible light present in an area. It helps the sensor determine how bright or dark the environment is. |
|
I |
Lux Level Threshold: Tap to set the threshold value for Lux ranges that determine when the sensor should activate. For more information, refer to Defining Lux settings. |
|
J |
Notify me if motion is detected: Tap the toggle switch to receive notifications when motion is detected. |
|
K |
Neutral wire fitted?: You can check if the neutral wire is connected during the device installation. The Wiser Home app automatically detects the wiring mode based on the installation, eliminating the need for manual selection.
|
|
L |
Identify: Tap
to identify the device. The status LED blinks red and the connected
light blinks on and off, upon successful identification. |
|
M |
Delete: Tap to remove the device from the system. NOTE:
|
|
N |
Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device. |