DUG_SmartMove Multiwire Dimmer Push_WH-01

Switching/Dimming the device manually

You can turn on/off and increase/decrease the brightness of the Motion Sensor Dimmer manually.

Short press the push button (< 0,5) once to switch on/off the Motion Sensor Dimmer.

Long press the push button (> 0,5 s) on the device to increase/decrease the brightness of the Motion Sensor Dimmer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?