Showing 11 - 20 of 272 results

Page 2 of 28
  • Innebygd automatisering

    ELKO - Smart ZB Termostat 16 A – Brukerveiledning for Wiser Home-enhet

  • Example of an automation

    ELKO - Smart Plug 16 A – Wiser Home Device User Guide

    Example of an automation Example of an automation Example of an automation In the example below, if away mode is enabled during Daytime, then Plug will turn off. Go to Automation > to create an automation. To add a condition, tap Add Condition > Away Mode > Enabled away mode (A). Read the
  • App Settings

    Elko Wiser Home – System User Guide (Norway)

    . Devices List of all Devices of your Home. Access to Device options. Away Mode Specify what happens when you activate the Away Mode, like temperature setting and which devices should be switched off. Refer to Away Mode for detailed information. System Settings More detailed Wiser Home App information
  • Creating an automation

    ELKO - SmartSensor Door/Win Wireless – Wiser Home Device user guide

    conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away Mode
  • Creating an automation

    ELKO - Smart Radiator Thermostat – Wiser Home Device user guide

    Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away
  • Troubleshooting

    ELKO - Motion Sensor Outdoor, 360 – Wiser Home Device user guide

    highly reflective surface. Ensure there are no swaying objects within the detection range. Check that the load is not wired directly to the power supply. Lighting turns on and off Quickly TIME set too short False trigger Wrong modes (Short pulse mode or Test mode) Ensure sensor is away from heat source
  • Bortemodus

    ELKO - Smart ZB Termostat 16 A – Brukerveiledning for Wiser Home-enhet

  • Creating an automation

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    triggers an action when at least one condition is met. Tap Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable / Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or
  • Bortemodus

    ELKO - SmartRadiatorTermostat – Brukerveiledning for Wiser Home-enhet

  • Creating an automation

    ELKO - SmartSensor Leakage Wireless – Wiser Home Device user guide

    conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable / Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away Mode
Page 2 of 28