DUG_SmartPlug 16A_ELKO_WH-00

Example of an automation

In the example below, if away mode is enabled during Daytime, then Plug will turn off.
  1. Go to Automation > to create an automation.
  2. To add a condition, tap Add Condition > Away Mode > Enabled away mode (A).
  3. Read the information and tap OK.
  4. To set the time, tap When > Add time > Period of time > Day time > Set.
  5. To add an action, tap Then > Add an action > Control a device > Smart Plug > Set.
    TIP: You can turn on/off the plug.
  6. Read the information and tap OK.
  7. Enter the name of the automation.
    TIP: You can choose the cover image that represents your automation by tapping .
  8. Tap Save.
    Once the automation is saved, it is visible on the Automation tab.
    NOTE: You can enable or disable saved automations on the Automation tab by using the toggle switch.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.