Showing 211 - 220 of 272 results

Page 22 of 28
  • About the device

    ELKO - SmartMove Relay 10A – Wiser Home Device user guide

    control the motion sensor switch through the Wiser Home app you will need the Wiser Hub. Direct operation: The motion sensor switch can always be controlled directly on-site. You can also connect any number of mechanical push-buttons. Functions Detection range. Automatic mode, manual operation.
  • Troubleshooting

    Elko Wiser Home – System User Guide (Norway)

    Hub. After pressing 3 times, the device LED blinks amber for 30 s. Pairing mode has changed. Press the Reset button on the device 3 times then hold for 20 s, until the LED blinks red. The device should reboot into the correct mode. The hub is not communicating or receiving updates. IPv4 is not
  • Changing the orientation of light sensors

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    Changing the orientation of light sensors Changing the orientation of light sensors Changing the orientation of light sensors You can change the orientation of the light sensors in the Wiser Home app. To change the orientation of the light sensors: In the Seasonal Comfort Mode set-up page, tap Light (LUX) sensors. Tap to see the available light sensors in Wiser Home app. Select the orientation in which the light sensors are facing and tap Set.
  • Creating a Schedule/Event

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    schedule, Frost Protection Mode will activate when the schedule begins. In Frost Protection Mode, the system maintains the room temperature at 5 °C to prevent freezing. WHEN: Set the time for the event (for example 12:00) You can create a maximum of 8 events per day. Copy Schedule: You can tap to copy
  • Changing the orientation of light sensors

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    Changing the orientation of light sensors Changing the orientation of light sensors Changing the orientation of light sensors You can change the orientation of the light sensors in the Wiser Home app. To change the orientation of the light sensors: In the Seasonal Comfort Mode set-up page, tap Light (LUX) sensors. Tap to see the available light sensors in Wiser Home app. Select the orientation in which the light sensors are facing and tap Set.
  • Sesongbasert komfortmodus

    Elko Wiser Home – Brukerveiledning for systemet (Norge)

  • Setting the room temperature using the app

    ELKO - Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing. When you add it to your Favourites. To know more about Favourite, refer to the Managing Favourite topic in the respective System
  • Changing the shutter orientation and location

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    Mode set-up page, tap Shutters. Update the orientation of the shutters and tap Set. If any shutter is covering a door, tap Yes I have shutters over a door to define its location. If no shutters cover a door, tap No. Select the shutters covering the doors from the list (A) and tap Finish.
  • Changing the shutter orientation and location

    ELKO - SmartBlinds Push – Wiser Home Device user guide

    Mode set-up page, tap Shutters. Update the orientation of the shutters and tap Set. If any shutter is covering a door, tap Yes I have shutters over a door to define its location. If no shutters cover a door, tap No. Select the shutters covering the doors from the list (A) and tap Finish.
  • Resetting the device

    ELKO - Smart Water Heater Puck – Wiser Home Device User Guide

    Resetting the device Resetting the device Resetting the device You can reset the device to factory default manually. Short press ( <0,5 s) the Setup/Reset button 3 times and then long press the Setup/Reset button once for 10 s to reset the Water heater to factory default mode. orShort press the
Page 22 of 28