ELKO - Smart Water Heater Puck_WH_00

Resetting the device

You can reset the device to factory default manually.
  1. Short press ( <0,5 s) the Setup/Reset button 3 times and then long press the Setup/Reset button once for 10 s to reset the Water heater to factory default mode.
    or
    Short press the push button 3 times a
    nd then long press the push button once for 10 s.
  2. After 10 s, LED starts blinking red then release the Setup/Reset button.
    NOTE: All configuration data, user data, and network data are deleted.
    The LED stops blinking upon successful reset of the device.
    The Water heater restarts and blinks green for a few seconds.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.