Showing 241 - 250 of 387 results

Page 25 of 39
  • Manual sensor settings

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    is installed and then press the O touch button for a few seconds to confirm the selection. The thermostat dot-matrix display the sensor type and LED flashes blue. Setting temperature calibration After selecting the floor sensor type, you must set the calibration value (offset value) of the sensor in
  • ELKO - Wiser Room Thermostat

    92500 Rueil Malmaison France elko.no/contact www.se.com Configuring the device Configuring the device Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Setting the device location Setting the device location You can add your device to any room (such as
  • Configuring the device

    ELKO - SmartMove Multiwire Dimmer Push – Wiser Home Device user guide

    the name of the device. B Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. C RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle
  • Using the device

    ELKO - Smart Smoke Alarm 230 V – Wiser Home Device user guide

    control panel page, you can see the following: Current state of the smoke alarm (A) History (B) The history page gives information about the smoke alarm (date, time, and type of alarm detected, for more information, refer to Checking the device history). Device settings (C) The smoke alarm setting page gives information about setting the LED brightness of the smoke alarm, for more information, refer to LED brightness settings. Add to favourites (D)
  • Using the device

    ELKO - Smart Smoke Alarm Battery – Wiser Home Device user guide

    control panel page, you can see the following: Current state of the smoke alarm (A) History (B) The history page gives information about the smoke alarm (date, time, and type of alarm detected, for more information, refer to Checking the device history). Device settings (C) The smoke alarm setting page gives information about setting the LED brightness of the smoke alarm, for more information, refer to LED brightness settings. Add to favourites (D)
  • Creating an Account

    Elko Wiser Home – System User Guide (Norway)

    account to have control over the Wiser system. Refer to the chapter Setting-up the Wiser System for information on how to setup the wiser system. If the homeowner decides to set up the Wiser system independently, they need to begin by creating an account before proceeding with setting up the Wiser
  • Roles in the Wiser Home App

    Elko Wiser Home – System User Guide (Norway)

    address and setting up the password Yes No Setting up the Wiser System Adding and configuring the hub and devices. Yes Yes Manual Firmware Update Updating the hub firmware manually No Yes Manage Rooms Add or delete Rooms Yes Yes Name or rename Rooms Yes Yes Manage devices Add or delete devices Yes
  • Innstilling av romtemperatur med appen

    ELKO - Smart ZB Termostat 16 A – Brukerveiledning for Wiser Home-enhet

  • ELKO - SmartBlinds Puck

    Hub to access and control the Puck. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Configuring the device Configuring the device Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France elko.no/contact www.se.com Setting the device location
  • Innstilling av sesongbasert komfortmodus

    ELKO - SmartSolskjerming Bryter – Brukerveiledning for Wiser Home-enhet

Page 25 of 39