Showing 31 - 40 of 86 results

Page 4 of 9
  • Håndtering av kabelen

    ELKO - Schneider Charge – Brukerveiledning for Wiser Home-enhet

  • Using the device

    ELKO - SmartSensor Climate Wireless – Wiser Home Device user guide

    Using the device Using the device Using the device The Control Panel of the sensor allows you to view the real-time temperature and humidity values. On the Control tab, tap All devices or a room tab where the sensor is located. On the sensor control panel page, you can see the following: The current temperature value (A) The current humidity value (B) History (C) Device settings (D) Add to favourites (E)
  • Using the device

    ELKO - SmartSensor PIR wireless – Wiser Home Device user guide

    Using the device Using the device Using the device The Control Panel of the sensor allows you to view if the motion is detected or not. On the Control tab, tap All devices or a room tab where the sensor is located. On the Sensor control panel page, you can see the following: Current lux level (A) Motion detection status (B) History (C) Device settings (D) Add to favourites (E)
  • Lademodus

    ELKO - Schneider Charge – Brukerveiledning for Wiser Home-enhet

  • Charging mode

    ELKO - Schneider Charge – Wiser Home Device User Guide

  • Setting alarms

    ELKO - Smart Water Heater Puck – Wiser Home Device User Guide

    new alarm. Select an alarm type. Overconsumption No consumption Select a device from the list (A) and tap Next. Enable the toggle switch (B) to set the alarm. Tap ( Watts) and enter a value to set a power limit. Tap ( During), select a time limit and tap Set (C). Tap Save. TIP: You can also turn the device ON/OFF when you add it to your Favourites.
  • Using the device

    ELKO - Smart Smoke Alarm 230 V – Wiser Home Device user guide

    control panel page, you can see the following: Current state of the smoke alarm (A) History (B) The history page gives information about the smoke alarm (date, time, and type of alarm detected, for more information, refer to Checking the device history). Device settings (C) The smoke alarm setting page gives information about setting the LED brightness of the smoke alarm, for more information, refer to LED brightness settings. Add to favourites (D)
  • Styring av persiennedrift uten temperatursensor

    ELKO - SmartSolskjerming Puck – Brukerveiledning for Wiser Home-enhet

  • Administrering av Matter-tilkobling

    Elko Wiser Home – Brukerveiledning for systemet (Norge)

  • Switching On/Off the device using app

    ELKO - Power Tag Control – Wiser Home Device User Guide

    control panel of the device and tap label to switch on/off the device. The control panel shows the current state of the device. If you only have single PowerTag in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen. TIP: You can also turn the device ON/OFF when you add it to your Favourites.
Page 4 of 9