DUG_PowerTag Control_ELKO_WH-00

Switching On/Off the device using app

Using the Wiser Home app, you can switch on/off the device.

On the Control tab, tap the power button to switch on/off the respective device

Alternatively, you can navigate to the control panel of the device and tap label to switch on/off the device.

NOTE:
  • The control panel shows the current state of the device.

  • If you only have single PowerTag in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.

TIP: You can also turn the device ON/OFF when you add it to your Favourites.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?