Showing 301 - 310 of 387 results

Page 31 of 39
  • Using the device

    ELKO - SmartDim LED Puck Multiwire – Wiser Home Device User Guide

    the sliding bar up/down to increase/ decrease the brightness. B Tap to manually turn the device ON/OFF. C Tap to redirect you to the Schedule screen, where you can create a schedule. For more information, refer to the Setting up a schedule topic. D Add to favourites Tap to add the device to the
  • ELKO - SmartSocket Double 16 A Wiser Home Device user guide

    eight loads at a time, which helps maintain the total consumption of thesystem below the established limit. This limit is determined by your contractspecifications, so it's important to refer to the Setting Tariff section for informationon peak and off-peak rates. Eligible devices will be
  • Using the device

    ELKO - SmartRelay Puck 10AX – Wiser Home Device User Guide

    open the Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. C Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. D Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.
  • LED Indications

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    simultaneously pressing O and + for 2 s to enter advanced settings menu. In advance setting menu the thermostat matrix display flashes P1 or P2... P9 when +/– button is pressed. Note: When + button is pressed, preset increases by one; similarly, the preset decreases by one when the – button is pressed
  • ELKO - smartplugg 16 A Brukerveiledning for Wiser Home-enheter

    under den fastsattegrensen. Denne grensen er fastsatt i kontraktsspesifikasjonene, så det er viktig åse i delen « Innstilling av tariff for informasjon om priser i perioder med høy og lavbelastning. Kvalifiserte enheter vil automatisk bli integrert i systemet for anti-tripping-administrasjon, noe som
  • Creating a moment

    ELKO - Power Tag Control – Wiser Home Device User Guide

    the Add actions menu, you can select the devices (C). Once the device are selected, tap Done. On the Moment creator page, tap on the device to set the preferred action (to turn on/off) and then tap Set on the upper right corner. After setting all actions, tap Save. Once the moment is saved, it will
  • Using the device

    ELKO - SmartDim Multiwire Universal LED Rotary – Wiser Home Device user guide

    increase/decrease the brightness of your dimmer. For more information, refer to Adjusting the brightness. B Tap to turn the device on/off. C Tap to open the Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. D Tap to add the device to the Favourite
  • Configuring the device

    ELKO - Smart Radiator Thermostat – Wiser Home Device user guide

    Climate Wireless), the system calculates the average temperature measured from all devices to control the heating based on the overall room temperature. If several Radiator Thermostats are installed in a room, the system uses the average temperature of all Radiator Thermostats.For more details, refer to the Setting the device as temperature source.
  • ELKO - Power Tag Control

    the Wiser Home app, you can configure the device according to your preferences. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 elko.no/contact www.se.com Setting the device location Setting the device location You can add your device to any room (such as
  • Using the device

    ELKO - SmartDim Multiwire Universal LED Push – Wiser Home Device user guide

    increase/decrease the brightness of your dimmer. For more information, refer to Adjusting the brightness. B Tap to turn the device on/off. C Tap to open the Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. D Tap to add the device to the Favourite
Page 31 of 39