DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

LED Indications

Pairing the device

Status

User Interaction

Description

Pairing in progress

The thermostat Dot-matrix display flashesJn to indicate that the joining process has started when the O touch button is pressed and held for more than 3 seconds.

Successful network joining

The thermostat Dot-matrix display flashes a green LED when the thermostat successfully joins a network.

Fails to join the network

The thermostat Dot-matrix display flashes a red LED when the thermostat fails to join the network.

Presetting the device

Status

User Interaction

Description

Enter preset selection

By default, thermostat matrix display flashes P5 if there is no external sensor connected, or P8 if there is any external sensor connected when the thermostat is first powered on or after a factory reset.

Modify preset selection

The default preset value can be modified by simultaneously pressing O and + for 2 s to enter advanced settings menu. In advance setting menu the thermostat matrix display flashes P1 or P2...P9 when +/– button is pressed.

Note: When + button is pressed, preset increases by one; similarly, the preset decreases by one when the button is pressed.

For more information, refer to the section presetting the device.

Setting a sensor type

Status

User Interaction

Description

Floor sensor type selection

The thermostat Dot-matrix display shows the floor sensor type and LED flashes blue.

Floor sensor calibration.

The thermostat Dot-matrix display shows the calibration value and LED flashes purple.

Floor temperature maximum limit

The thermostat Dot-matrix display shows the maximum temperature limit and LED flashes red.

Resetting the device

Status

User Interaction

Description

Soft reset

A solid Sr LED is displayed on the thermostat Dot-matrix display until the user releases the O button, then Sr flashes. For more information, refer to the section Resetting the device.

Factory reset

A solid Fr LED is displayed on the thermostat matrix display until the user releases the O button, then Fr flashes. For more information, refer to the section Resetting the device.

Showing demand - temperature control modes

Status

User Interaction

Description

Heating demand

The Dot-matrix display shows a solid red LED to indicate the thermostat is heating when the setpoint is higher than the current room temperature.

Temperature display

Status

User Interaction

Description

Temperature below minimum display value
OR
Temperature reading error.

Note: The thermostat Dot-matrix display shows the temperature limits -9 °C to 99 °C.

The thermostat matrix display flashes -- When the temperature is below -9 degrees.

OR

The thermostat matrix display flashes -- when the thermostat cannot determine the temperature due to an error.

Temperature above maximum display value

Note: The thermostat Dot-matrix display shows the temperature limits -9 °C to 99 °C.

The thermostat matrix display flashes + + when the temperature is above 99 degrees.

Away mode

Status

User Interaction

Description

Away mode is set in ELKO app.

A dot-matrix display glows, indicates that the thermostat is in away mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.