DUG_Smart Radiator Thermostat_WH-00

Configuring the device

IMPORTANT: The temperature data from the Radiator Thermostat sensor will be used as an input for the room’s heating system. If a room has an additional temperature measuring device (such as a Room Thermostat, Smart ZB Thermostat 16A, or SmartSensor Climate Wireless), the system uses that device for temperature measurement because it is typically placed in a more representative location than the radiator thermostat. Finally, if a room has multiple temperature measuring devices (Room Thermostat, Smart ZB Thermostat 16A, or SmartSensor Climate Wireless), the system calculates the average temperature measured from all devices to control the heating based on the overall room temperature.
  • If several Radiator Thermostats are installed in a room, the system uses the average temperature of all Radiator Thermostats.

For more details, refer to the Setting the device as temperature source.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.