Showing 91 - 100 of 272 results

Page 10 of 28
  • ELKO - SmartSocket Double 16 A Wiser Home Device user guide

    detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. For more informationabout Away Mode, refer to the system user guide. NOTE: Maximum 10 conditions can be added. New automation If When Conditions
  • Selecting the operating mode

    ELKO - SmartSensor Door/Win Wireless – Wiser Home Device user guide

    Selecting the operating mode Selecting the operating mode Selecting the operating mode Using the Wiser Home app, you can select the operating mode for the sensor such as window or door. On the Home screen, tap icon. Tap Devices Window/Door Sensor Operation Mode (A) to select one of the following
  • Setting boost mode manually

    ELKO - Smart ZB Thermostat 16 A – Wiser Home Device user guide

    Setting boost mode manually Setting boost mode manually Setting boost mode manually You can manually enable and disable the boost mode.When enabled the temperature increases by 2° C for temperature control modes (P1 to P8) and by +2 for regulator mode (P9) over the current temperature. To enable
  • ELKO - SmartRelay Puck 10AX Wiser Home Device User Guide

    Puck 10AX 4. Tap Add conditions (B) and select any of the following (C): – Device status change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can
  • Troubleshooting in Quick Home Connect

    ELKO - SmartSwitch Push Wireless Plus – Wiser Home Device User Guide

    SmartSwitch push SmartRelay puck Multiwire puck dimmer SmartBlind puck Push-button dimmer Rotary dimmer Socket outlet SmartBlind push Double socket outlet Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in
  • Troubleshooting in Quick Home Connect

    ELKO - SmartRelay Puck 10AX – Wiser Home Device User Guide

    puck Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing Pair the device again. Refer to SmartRelay puck The Wireless switch
  • Troubleshooting in Quick Home Connect

    ELKO - SmartDim LED Puck Multiwire – Wiser Home Device User Guide

    Puck Dimmer Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing Pair the device again. Refer to Multiwire Puck Dimmer The Wireless
  • Troubleshooting in Quick Home Connect

    ELKO - SmartBlinds Puck – Wiser Home Device user guide

    puck Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing Pair the device again. Refer to SmartBlind puck The Wireless switch
  • Troubleshooting in Quick Home Connect

    ELKO - SmartSocket Single 16 A – Wiser Home Device user guide

    Socket Outlet Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing Pair the device again. Refer to Single Socket Outlet The Wireless
  • ELKO - Schneider Charge Wiser Home Device User Guide

    one of the condition must be met to trigger an automation. 5. Tap Add conditions (C) and select any of the following (D): – Device status change (Select the device)– Away Mode (Enable or Disable)– Energy Price changes (To define the energy price limit.) NOTE: This condition is available only if your
Page 10 of 28