DUG_ELKO - Smart ZB Thermostat 16 A_WH-00

Setting boost mode manually

You can manually enable and disable the boost mode.
When enabled the temperature increases by 2° C for temperature control modes (P1 to P8) and by +2 for regulator mode (P9) over the current temperature.

To enable boost mode:

  1. Press O button once to enter boost menu.


    +1 flashes on Dot-matrix display.
  2. Use the +/- button to navigate between the boost hours from +1 to +3.

    If there is no interaction for 5 seconds, the thermostat saves the selection and exits Boost Mode automatically.

For example:
If the ambient temperature is 20° C and the set point is 18° C, there is no heat demand. To temporarily increase the temperature, you can enable Boost Mode. When Boost Mode is active, the setpoint becomes 22°C (current temperature + 2°C) for the selected boost duration. After the boost period ends, the setpoint returns to its original value (18°C) or to the scheduled value if scheduling is enabled.


To disable boost mode:

  1. Press O button once.
    +1 flashes on thermostat Dot-matrix display.

  2. Press + button for thermostat to display – – (boost cancel).

    After selecting the boost cancel, thermostat will save and exit boost mode if there is no interaction within 5 s.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.