ESXP2GE006EN-05

Architectures for Arc Flash Protection as an Autonomous Feature

Below is the recommended digital architecture for the Arc Flash Protection application when PowerLogic A125 / Arc V121 performs arc fault protection autonomously from the electrical protection relay.

NOTE: For more information about options for Arc Flash Protection in LV switchboards, refer to Arc Flash Protection System in iPMCC by OKKEN Design guide (document number AFPDG0120EN).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?