ESXP2GE006EN-05

Data Processing

Arc Flash Protection

To help ensure fast reaction to arc flash, data processing of light and current sensors is performed locally by the arc flash protection system that will trigger the circuit breaker opening (PowerLogic P5 30 series, P3 Advanced, or PowerLogic A125 / Arc V121).

Smart Clustering

To obtain a contextualized capture of the arc flash incident, data processing in Edge Control software consists of:

  • Consolidation of alarms, events, waveforms, status changes, and other corresponding data from all connected products in chronological views

  • Smart grouping of related data to help identify the root cause of incidents

Smart clustering is performed by EcoStruxure Power Monitoring Expert or Power Operation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?