0100DB2326

Context of Application

Today’s building owners are facing increasing pressure to make their facilities operate more efficiently on multiple fronts. Energy prices certainly remain high in many regions and are the primary driver for businesses seeking to lower their ongoing operating costs. More recently, energy efficiency regulations also have been pushing owners to understand and begin reducing their energy use.

Problem to Solve

The facility/energy manager needs to:

  • Demonstrate compliance with standards related to energy efficiency (ISO 50001, 50002, 50006, Superior Energy Performance® , NEC 220.12, ASHRAE 90.1, CA Title 24, IECC, LEED, and other local/regional energy efficiency standards).

  • Communicate the energy efficiency program to stakeholders, and report on energy performance improvements.

Purpose of the Application

Enable a systematic approach to achieving continuous energy performance improvement

  • By making energy usage visible at all stages of an energy management and improvement plan.

  • By providing transparency through reporting on energy performance indicators (EnPI) to regulators or shareholders, and demonstrating continuous improvement.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?