0100DB2326

Outputs

Live Data Display

Measured energy values such as kWh and peak demand (kW) highlighted in ISO 50006 sub-standard of ISO 50001 can be displayed in dashboards, custom graphical diagrams, and live data tables in EcoStruxure Power Monitoring Expert or Power Operation (refer to Energy Monitoring application).

Events and Alarms

Smart alarms can be configured to alert energy managers or operations staff in case of energy-related events which require attention (imminent exceeding of peak demand threshold, etc.) (refer to Energy Monitoring application).

Trends

Measured energy values, ratios of measured values, or KPIs (kWh/unit of production, etc.) can be trended in the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation).

NOTE: To monitor ratios of measured values in trends, normalization data such as production, temperature, square meters, etc. must be integrated using ETL, OPC or .csv file export. In addition, the KPI Report must be configured to write KPI data into the database in EcoStruxure Power Monitoring Expert or Power Operation (refer to Energy Monitoring application).

Dashboards

Dashboards to visualize, analyze, and communicate energy performance in accordance with an ISO 50001 management program can be configured (refer to Energy Monitoring application).

Some examples of dashboards include:

  • Sankey diagram

  • Energy heatmap

  • Pareto chart

  • Period over period

  • Historical trends, bar chart, line chart with target line, pie chart

  • KPI dashboards (Energy Intensity*, etc.)

Reports

Several reports are available to support Energy Efficiency Compliance:

  • Consumption Ranking Reports

  • Energy Comparison Reports

  • Energy Modeling Reports

  • Energy Usage Reports

  • Calendar Trend Reports

  • KPI Engine Reports

  • Load Profile Reports

  • Energy Cost Reports

These reports are described in detail in the Energy Monitoring application.

To help evaluate the effectiveness of energy saving initiatives, an energy model can be created to simulate the facility's energy baseline. This baseline can then be compared to energy drivers such as production, heating, or cooling degree days. It analyzes actual energy use compared to the model to track and forecast energy savings as a result of organizational or operational changes (refer to Energy Modeling and Verification application).

Notifications*

SMS or email notifications are sent on pre-alarm and alarm conditions described above to enable fast action.

Cloud-Based Analytics and Services

As an option, EcoStruxure Service Plan powered by EcoStruxure Power Advisor provides data quality analytics with recommendations from our Schneider Electric service experts.

For further information, refer to Data Quality Management.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?