0100DB2313

Digital Architecture

The digital architecture of the Power Event Analysis application involves collecting the input data from the different products, either directly over Ethernet or via gateways. This data is then used by the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation) for on-premise visualization analysis and reporting.

The most significant factors in the customer process can also be captured from external process software using the OPC standard or ETL tool.

As an option, EcoStruxure XR Operator Advisor Client can be used to enhance the Power Event Analysis application with virtually overlaid data on top of equipment and devices.

Data from EcoStruxure Power Monitoring Expert or Power Operation can be passed on to the EcoStruxure Power Advisor platform and interpreted by experts as a part of the EcoStruxure Service Plan.

The recommended digital architecture for the application is shown below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.