FDM121 Front Display Module for One Circuit Breaker
The FDM121 display shows the measurements, alarms, and operating assistance data from the intelligent modular unit (IMU). The FDM121 display can control a circuit breaker that is equipped with a motor mechanism or with the pre-defined application performed by the IO module.
The FDM121 display with part number TRV00121 or STRV00121 is compatible with the following ranges of circuit breaker:
-
MasterPact MTZ circuit breakers
-
MasterPact NT/NW circuit breakers
-
ComPacT NS circuit breakers
-
ComPacT NSX circuit breakers
-
PowerPacT P- and R-frame circuit breakers
-
PowerPacT H-, J-, and L-Frame circuit breakers
-
The information related to the new generation of ComPacT NS and PowerPacT P- and R-frame circuit breakers in this document applies to the existing range ComPact NS and PowerPact P- and R-frame circuit breakers also. The exceptions are mentioned wherever applicable.
-
The information related to the new generation of ComPacT NSX and PowerPacT H-, J-, and L-Frame circuit breakers in this document applies to the existing range ComPact NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.
-
These new ranges are based on the same technical and dimensional architecture as that of the existing range of circuit breakers.