DOCA0150EN-08

Firmware Version 004.000.009

New Features

Supports MasterPact MTZ circuit breaker and provides the following features:

  • Metering

  • Breaker status and control

  • Device identification

  • Reset (peak demand values, energy meters, minimum and maximum values)

  • Maintenance (operation counters, load profile)

NOTE: Alarm History and New event pop-up features are not available for MasterPact MTZ circuit breaker.

QR code for this page

Was this helpful?