990-6400C-001

Final Installation

  1. Reinstall the protection cover in front of the non-Class 2/non-SELV terminals.

    250-300 kVA UPS

    400 kVA UPS

  2. Reinstall the signal cable covers.
  3. Reinstall the plates.
  4. Install the kick plates.
  5. Close the door.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.