990-6400C-001

Route the Signal Cables

Recommended signal cable size is 0.5-0.8 mm2.
  1. Remove the signal cable covers from the UPS.

    250-300 kVA UPS

    400 kVA UPS

  2. Route the Class 2/SELV signal cables through the top opening(s) and down to the Class 2/SELV terminals as shown.

    250-300 kVA UPS

    400 kVA UPS

  3. Route the non-Class 2/non-SELV signal cables through the top right opening and down to the non-Class 2/non-SELV terminals as shown.

    250-300 kVA UPS

    400 kVA UPS

  4. Fasten the signal cables with cable ties.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.