990-91384E-001

Installation Procedure

WARNING
heavy load
The UPS is tall and heavy. Take appropriate precautions when handling the UPS.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Single System

Parallel System

  1. Connect the Power Cables.
  2. Route the Signal Cables. See Signal Connections for signal details.
  3. Only for parallel system: Connect the Parallel Cables in a Parallel System.
  4. Optional: Connect the Synchronization Cables between Two UPS Systems.
  5. Final Installation.
For moving or decommissioning the UPS after installation has been completed, see Decommission or Move the UPS to a New Location.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?