990-91384E-001

Route the Signal Cables

  1. Remove the signal cable cover from the UPS.
  2. Route the Class 2/SELV signal cables through the top left entry opening and down along the front plate to the connection points.
  3. Remove the protection cover in front of the non-Class 2/non-SELV terminals.
  4. Route the non-Class 2/non-SELV signal cables through the top right opening and down to the non-Class 2/non-SELV terminals as shown.
  5. Fasten the signal cables with cable ties as shown.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?