990-915757-001

Safety Precautions

WARNING
Hazard of electric shock, explosion, or arc flash
  • Do not unpack the units before the time of installation.
  • Cover the units and store the units in a temperature controlled indoor environment free of conductive contaminants and humidity, where the units are protected from moisture until the time of start-up. Moisture inside the cabinet can create hazardous short circuits.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
Heavy load
The product is large and heavy (4800 kg (10582 lbs)). Use appropriate lifting equipment and trained personnel to lift the product.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?