990-91463B-001

3:3 IT System Single Source and Single Mains

NOTE: Refer to IEC 60364 series for general requirements and refer to local codes for specific local requirements.
NOTE: By impedance grounding, the UPS system is connected to the mains supply ground via an impedance.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.