990-91463B-001

3:3 TN-S System Dual Source and Dual Mains

NOTE: Refer to IEC 60364 series for general requirements and refer to local codes for specific local requirements.
NOTE: In regions where neutral is not allowed to be disconnected per local regulations, use a 3-pole circuit breaker.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.